I am testing out the new default SD card environment for EZSDK 5.03.00.09. I have created an SD card using the mksdboot.sh script and tried to boot with this. U-Boot seems to load fine as "version" shows: "U-Boot 2010.06 (Nov 10 2011 - 19:25:12)".
I run "mmc init" then "fatload mmc 0 0x80009000 uImage" but it fails with:
TI8168_EVM#fatload mmc 0 0x80009000 uImage
mmc_send_cmd: timedout waiting for cmddis!
** Can't read from device 0 **
** Unable to use mmc 0:1 for fatload **
Please can someone help? I feel there is an issue with the bootloader itself. Surely a buggy U-Boot hasn't been shipped with the EZSDK?
Thanks,
Ralph