Hi TIers,
I'm using DM8168 with RDK3.0
I modify
file : dvr_rdk/mcfw/src_bios6/links_m3vpss/swMs/swMsLink_drv.c
function : Int32 SwMsLink_drvDoDma(SwMsLink_Obj * pObj, FVID2_Frame *pFrame)
thickness = 1;
to set the width of swms grid to 1,
booting up failure
Log Infomation
3771.Log_3.0_1_10_3_20140730_0945.txt
But when the width be set to 4,3 or 2, it works properly,
when the width be set to 1 in RDK4.0, it works properly also.
How can I fix this issue, when the width be set to 1 in RDK3.0
Best Regards!