Hi.
I'm using DVRRDK 3.5. My usecase is as follow.
1080p30 4CH Capture ---> Resize(1080p, 720p, etc..) --> encode
|-> swMs --> display
I know that one scalar's capablity is upto 1080p30 * 3. So. i should use 2 scalars for encoder.
But, if I use 2 scalar for encoding. swMs can't be created.
I use DEI single output scalar for encoder.
According to RDK source code, VPS_M2M_INST_MAIN_DEIH_SC3_VIP0 / VPS_M2M_INST_AUX_DEI_SC4_VIP1 are used.(maybe SC3 & SC4. Correct?)
In this case only SC5(SYSTEM_SW_MS_SC_INST_SC5) is OK, and the other scalar instance makes assertion error.
Is this usecase possible? If possible, how should i assign scalars for encoder & swMs?