We've run into an interesting problem where the qualiTI tool passes our algorithm in one Linux setup and not the other. We isolated the problem to a run error when attempting to run the sectti script on the results of ofd6x (CG XML tools 2.12.00, from DVSDK 2.00 for HD DaVinci). When we do so, we get the above error message.
When we try running the same sectti on our O3530 setup on the same ofd6x output (same 2.12.00 version of CG XML, but not on Ubuntu), it works fine. Also, other qualiTI tests involving ofd6x pass on Ubuntu. This leads us to believe the issue is with running sectti -- and, more specifically, running sectti on this particular setup.
We are using Ubuntu running on VMWare for HD DaVinci.
This becomes a problem for us because we've found that the RTSC genpackage tool runs into the same issue and is therefore not able to extract the linker sections that it should (causing a problem later for genserver).
We tried using CPAN to get the latest versions of XML::Parser and XML::Simple. It indicates the latest is installed.
We can try working around this by using our O3530 setup to run genpackage and doing the HD DaVinci specific genserver command for the rest of the packaging/testing flow (or trying something besides Ubuntu to run HD DaVinci DVSDK 2.00). Thought I'd check to see if anyone else has run into this issue and, if they have, how they got around it.
Thanks!
-Robert