Hi,
I'm using the EVM (revision I) for OMAPL137. I'm trying to install the SDK software by following the wiki page:
http://processors.wiki.ti.com/index.php/Installing_the_Software_for_OMAP-L137
I've put the six .bin files in /tmp
- OMAPL137_arm_setuplinux_#_#_#_#.bin
- bios_setuplinux_#_#_#.bin
- xdctools_setuplinux_#_#_#.bin
- LPTB-#_#_#_#-beta.bin
- mvl_5_0_#_demo_sys_setuplinux.bin
- ti-cgt-C6000_#.#.#_setup_linux_x86.bin
In the "Installation Steps" part, it " strongly recommend that you change the default installation locations to place the components together" and gives an example:
Execute the SDK installer that you previously downloaded from the OMAP-L137 Software Download page in a temporary directory.
- For example:
- host $ cd /tmp
- host $ ./OMAPL137_arm_setuplinux_#_#_#_#.bin
- NOTE: If you do not have a graphical display, you may use console installation with the following command.
- host $ ./OMAPL137_arm_setuplinux_#_#_#_#.bin --mode console
- Path Information - This installs the DVSDK in /home/<useracct>/OMAPL137_arm_#_#_#_#
I'm wondering how to change the default installation path, I put the command "./OMAPL137_arm_setuplinux_#_#_#_#.bin --mode console" in terminal and also tried to switch to console mode by ctrl+alt+F1 then put "./OMAPL137_arm_setuplinux_#_#_#_#.bin". But nothing happened. Neither way prompts me any path information. And I cannot find anything(by using "find" and "locate" command) under the expected path either. I'm new to this, please help me with it. Thank you!