Hi,
I have some problems with binding image to a device on secure device.
I have a DSP_ubl_ais.bin image, which is burned into NOR FLASH, and i can call secure kernel's API to encrypt the
CEK struct head. And then write encrypted CEK struck back to where just read it. NOR flash's drivers are work well.
After write CEK's struck back to nor flash, power off device, and then power on device, i can't see any informations on PC terminal.
following is my ini file
; *********************** INI ************************
; General settings that can be overwritten in the host code
; that calls the AISGen library.
[General]
; Can be 8 or 16 - used in emifa
busWidth=16
; SPIMASTER,I2CMASTER,EMIFA,NAND,EMAC,UART,PCI,HPI,USB,MMC_SD,VLYNQ,RAW
BootMode=EMIFA
; NO_CRC,SECTION_CRC,SINGLE_CRC
crcCheckType=NO_CRC
; Security settings (keys, options, list of sections to encrypt, etc.)
[Security]
; Security Type: GENERIC, CUSTOM, NONE
securityType=GENERIC
; Boot Exit Type: NONSECURE, SECUREWITHSK
; NONSECURE = Device switches from secure type to non-secure type, jumping to loaded code
; (no secure kernel since no longer secure device).
; SECUREWITHSK = Device remains as secure type, secure kernel is loaded, allowing run-time
; security context switching.
bootExitType = SECUREWITHSK
; Encrypt section list (ALL or comma-separated list of section names)
encryptSections=ALL
; CEK used for AES encryption of data - must be string of 32 hexadecimal characters
; Device uses KEK to encrypt CEK, and then SECURE KEY LOAD command load this CEK, uses to
; decrypt the data by ENCRYPTED SECTION LOAD command
encryptionKey=4A7E1F56AE545D487C452388A65B0C05
;encryptionKey=0123456789abcdeffedcba9876543210
; SHA Algorithm Selection
genericSHASelection = SHA1
; This section allows configuration of one the systme IOPUs.
; The iopuNum field must be valid (0-5) and then mppaStart
; and mppaend fields allow setting a range of mppa MMRs to the
; same supplied mppa value.
; IOPUSELECT: | RSVD | iopuNum| mppaStart | mppaEnd |
; MPPAVALUE: | mppaValue |
[IOPUCONFIG]
IOPUSELECT = 0x000000FF
;MPPAVALUE = 0xFFFFFFFF
MPPAVALUE = 0x80
[AIS_Set]
; Generic AIS set instruction to a reserved register to force a signature check
TYPE=2
ADDRESS=0x01E2C020
DATA=0
SLEEP=0
[IOPUCONFIG]
IOPUSELECT = 0x000100FF
;MPPAVALUE = 0xFFFFFFFF
MPPAVALUE = 0x80
[IOPUCONFIG]
IOPUSELECT = 0x000200FF
;MPPAVALUE = 0xFFFFFFFF
MPPAVALUE = 0x80
[IOPUCONFIG]
IOPUSELECT = 0x000300FF
;MPPAVALUE = 0xFFFFFFFF
MPPAVALUE = 0x80
;This will set all security bits in IOPU6 registers to unlock security
;protection on all IOs protected but will lock the SYCFG registers to
;access only by secure supervisor ROM or secure kernel.
[IOPUCONFIG]
IOPUSELECT = 0x000600FF
MPPAVALUE = 0xFFFFFFFF
;This will set bit 7 of IOPU6 to 0 that will unlock the security protection
;on SYSCFG registers which is ideally what you need to configure PINMUX and
;other system registers.
[IOPUCONFIG]
IOPUSELECT = 0x00060707
MPPAVALUE = 0x00000000
; This section allow setting the MPU1 or MPU2. If the
; rangenum is out of the allowed range then all the ranges
; (including the fixed range) take the start, end, and
; protection values.
; |------24|------16|----------8|----------0|
; MPUSELECT: | RSVD | mpuNum | rangeNum |
; STARTADDR: | startAddr |
; ENDADDR: | endAddr |
; MPPAVALUE: | mppaValue |
[MPUCONFIG]
MPUSELECT = 0x000001FF
STARTADDR = 0x00000000
ENDADDR = 0xFFFFFFFF
MPPAVALUE = 0xFFFFFFFF
I follow the demo's process,:
step 1:
Uint16 usNorArry[NOR_BLOCK_SIZE];
magicWord = (Uint32 *)&usNorArry[2]; //AIS magic number (1 word)
AISKeyLoad = (Uint32 *)&usNorArry[4]; //AIS key load command (1 word)
pUserKey = (SL_usrKeyStruc *)&usNorArry[6]; //AIS key header (8 words)
AISExitType = (Uint32 *)&usNorArry[22]; //AIS set exit type (2 words)
pDutyCmd = (Uint32 *)&usNorArry[26]; // AIS func command + params (12 words )
AISSetCmd = (Uint32 *)&usNorArry[50]; //AIS set command + params (5 words)
pSigData = (Uint32 *)&usNorArry[60]; //Signature (16 words)
step2:
Create the Initialization vector (IV) for the encryption, and then call secure kernel API SK_setUserKey to encrypt CEK ,
step3:
Create the hash of the encrypted header.
And in this point, shall me update the pDutyCmd data by calling SHA_update function?
SHA_update(currHashAlgorithm, &ctx, (Uint8 *) pDutyCmd, sizeof(Uint32) * 12);
step 4:
Encrypt the digest for the signature.
Step 5:
write back into nor flash .
And then power off device, and power on device again.But there is nothing spits to PC terminal.