Dear All,
I am looking for an EVM Board/Experimenter's Kit/Development Board which has a upp connection. I want to connect high speed (>100Msps, 14-16 bit) ADC and DAC to the board.
The setup will finally be a software defined radio (SDR) which can directly synthesise, analyse, receive and transmit communication signals in the 1 - 30 MHz band.
It seems that TI OMAP-L138 LCDK does not support upp connectivity.
I would appreciate it very much if you could recommend an OMAP-L138 EVM Board/Experimenter's Kit/Development Board with a upp port. It would be great if you could also recommend an ADC/DAC board with the above specs.
Regards,
Cenk.