Hello,
I am trying to use the OMAP-L138 DSP+ARM9 LCDK to run the experiments in the book by Donald Reay for the first time. I went to chapter 2 to find the sine48 example since I couldn't see it in Chapter 1, (only a dotp4 project and the source code for sin48). Then I tried importing the project (the one in chapter 2) but CCS complained about overlapping workspaces, then I created a different workspace (with a different name) and imported the project. When the project opens I get this error below. I am using CCS Version: 5.5.0.00077. I am connecting the LCDK to the Host PC via UART-USB. Can someone please tell me what the problem is here?. Am I not using the right LCDK for this project?, or is there another problem?. Thank you,