Hi !
I've got the OMAL-L137 EMV from Spectrum Digital...
I've also got some nice running in Emulation mode through CCS. This code is intended to run on the DSP and I do not yet explicitly do anything with the Arm...
Does this mean I can generate an AIS with AISgen from the .out file and simply flash that ? Do I have to indicate to the Dev Board whether it has been flashed it to NAND or SPI ?
Also, what changes about this process if I want to use the ARM running Linux to read from the SSD card and send that information to the DSP ?
Thanks,
Amanda