Hi, everyone.
I have a board using AM1808 made by some company which is not available now.
I am porting linux 2.6.3 kernel.
I have a circuit diagram of the board.
In the board, UART1/2 are used for debug and RS-485.
But UART0 is assigned to WiFi daughter board connector.
I think UART0 pin may be assigned for WiFi connection.
I checked by inputing "echo asdjfkdsf > /dev/ttyS0" by console, no signal on UART0 pin.
How can I check this UART0 RX/TX pins are assigned to which function?
How can I assigned UART0 RX/TX pins for UART0?
I don't have a plan to use WiFi function.
Kernel? or u-boot?
BR
Paul