I am working on a lot of curriculums to get well acquainted with the OMAP-L138 and its applications, I got several teaching courses that
I am following; Nevertheless, I am still not capable to successfully build the "mcaspPlaybk.c" as I am facing errors that, I believe related with the libraries. whereas the same thing happened for the L138_aic3106_init.c .and L138_aic3106_init.c .
I know adding library supposed to be an easy task but every time the number of errors get doubled and trippled, please help me out at least with mcaspPlaybk.c or in case of examples in the book "Digital_Signal_Processing_and_Applications_with_the_OMAP_L138_eXperimenter" although I followed the instructor step by step, over and over again but failure is only what I got as I am facing the same problems when it comes to the building step.
in the L138_aic3106_init.h . although I added "C:\eXperimenter\1020489B-1_CCSv4-2-4_with_SOM-M1_BSL_WS_2\CCSv4-2-4_with_SOM-M1_BSL_WS\DSP BSL\inc" to the lnclude option, which it contains all the "evmomapl138.h" but still I got the following error "..\L138_aic3106_init.h", line 7: fatal error: could not open source file "evmomapl138.h"
I really want to solve those problems out,
I am using CCS.5.2.1.00018 and the following libraries packages:
- C6748_StarterWare_1_20_03_03
- 1020489B-1_CCSv4-2-4_with_SOM-M1_BSL_WS_2
- c674x-dsplib_1_03_00_01 -
- OMAP_L138 starterWare
thanks ever such a lot in advance