Hi
I am trying to install CCS v6.1.2 (ccs_setup_6.1.2.00015.bin) on Linux Kubuntu 13.10.
I am following the instructions in README_FIRST.txt file and the platform specific instructions on TI wiki.
sudo apt-get update gives me tens of the following type of errors:
W: Failed to fetch http://security.ubuntu.com/ubuntu/dists/saucy-security/multiverse/binary-i386/Packages 404 Not Found [IP: 91.189.91.14 80]
And I am assuming that the previous error is the reason why the consecutive step with "sudo apt-get install libgnomeui-0 libusb-1.0-0-dev" also fails.
Do you have working instructions on how to install the CCS6 on Ubuntu 13.10? The ones in TI wiki do not work. Do you have those missing packages available in some repository?
Marko