All:
I am sure that there are several enhancements that have been considered - but here is one:
If you had extended the pins on the J14, J15 headers it would allow me to easily connect a logic analyzer to the EMIFA bus or other specific communications buses to follow on the LA what is going on with the hardware. Is that something that could be done for a future pass of the board?
Also, it would be nice to have a built-in emulator on the board, like the TI Launchpads have. (I realize there is a LOT of hardware on the board, but it does add to the "low cost" to have to procure an emulator.)