Other Parts Discussed in Thread: OMAPL138
Tool/software: TI-RTOS
Hello,
I am working on a project that uses the OMAP-L137 as the main application processor. We will use both, ARM9 and the DSP CC674x in it in our use-case.
I wish to use TI’s RTOS for evaluating it’s USB device side driver performance.
I am confused between DSP/BIOS and SYS/BIOS packages. And then there is a TI-RTOS package also.
Which one of the above 3, and within them which version of it will support OMAP-L137, including USB Device side drivers?
Also, which compatible CCS version should I be using with it?
I have a registered account in TI and please guide me to the links of the supported RTOS and CCS to make OMAP-L137 boot and be able to use USB device-side drivers.
I appreciate your help.
Regards,
Yusuf Husainy.