Regarding Table 5-14 "EDMA Synchronization Events" in the OMAPL138B-EP data sheet (SPRS815C, revised April 2013), the following synchronization events are labelled "Reserved".
EDMA3 Channel Controller 1: 19, 20, 21, 22, 23, and 30, 31
I interpret this table to indicate there are no peripheral interface events that will trigger synchronization events for channels 19, 20, 21, 22, 23, and 30, 31 on EDMA3 Channel Controller 1.
Is it safe to use those channels (19, 20, 21, 22, 23, and 30, 31) from EDMA3 Channel Controller 1 for chained transfers or "manually" triggered transfers?
Or should I steer clear and use other channels?
Would you expect things to work out for me if I used a hardware interrupt on a GPIO line in bank 8 to fire EDMA3 Channel Controller 1 synchronization event 18 (GPIO Bank 8 Interrupt) to trigger a transfer on EDMA3 Channel Controller 1 channel 18, which then triggers chained transfers on channel 19, then 20, then 21, etc.?