Hi,
When I power on my OMAP L138 EVM, without initializing any parameters, the ehrPWM output (pin J15.44) is showing 3.3v on my oscilloscope. This indicates that the OMAP L138 LCDK, by default generates high logic output for its ehrPWM. After I program my code and run it in CCS, I can control the output of ehrPWM.
However, we need to make the default value low. I would like our OMAP L138EVM to generate no signal when its powered on.
Any idea how to achieve this?
Thank you