This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Currnet my 'battery' (power supply connected currently) is showing 0%
1)How do I reset the charge to someting arbitray like 90%?
2)I'm trying to configure interrupts. In my reading soc delta = 0, implies rsoc interrupts are off. Though on the bqstudio I set SOC Delta = 0, write, and then if i reset it goes back to one. I do not see the interrupt clear. How do I turn this off through the gui?
After further experimentation soc delta ON THE GUI is not sticky. Looks like it doesn't write to flash. Thus you can't disable it.
I was able to manually write to flash with my own code and disable it. This is the only way I could disable the interrupt.
Likewise the io Config does not appear sticky either...
mmmm...actually might of been below flash write voltage...
Hello Craig,
Yes. If voltage is below flash write voltage then changes to data flash will not write.
Regards,
Nick