This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Screen Allignment problem with S Video connectivity on TV using Beagle board XM Rev B



Hi All,

 

We have successfully loaded OMAP3/4 Maverick 10.10 Linux image to Beagle Board XM Rev B with SD card (4GB) as the boot source.

For changing the display screen to a TV output with S-Video connectivity, we changed the bootargs for NTSC as per

http://elinux.org/BeagleBoardUbuntu#S-Video

The S-video output is enabled by changing the bootargs at Uboot as given below.

omapfb.mode=tv:ntsc

omapdss.def_disp=tv

The Bootargs are also validated in Boot.scr file as shown below.

Setenv bootargs 'console=tty0 console=ttyS2,115200n8 root=/dev/mmcblk0p2 rootwait ro vram=12M omapfb.mode=tv:ntsc omapdss.def_disp=tv fixrtc buddy=unknown'

With the above settings, we were able to see the display output on a S-Video enabled TV.

However, around 10% of the left and right margins of the screen are out of display.

The same S-Video (screen mis-alignment) problem was observed with PAL settings also.

Any thoughts or pointers on how this issue could be fixed is highly appreciated.

Regards,

Ajish S ,

Embedded Design Engineer.