Is the newest incarnation of the MMC/SD/SDHC card, namely SDXC supported by the OMAP3530 hardware?
What changes, if any, are required in the omap_hsmmc driver?
Thanks very much, Chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the newest incarnation of the MMC/SD/SDHC card, namely SDXC supported by the OMAP3530 hardware?
What changes, if any, are required in the omap_hsmmc driver?
Thanks very much, Chris
Based on what i read on SDXC, it is supported using the SD 3.0 specification and its higher capacities need to use SD 4.0. The OMAP3530 hardware only supports SD v2.0. I don't think it's just a matter of changing the driver, the h/w fundamentally wouldn't be able to support it.
Regards,
James