hi
Now I have a trouble about C6455 SRIO.
In follow two assumed cases:
1. In a SRIO system, there are two C6455 devices, which is connected each other directly through SRIO BUS, one as HOST device, the other as SLAVE device. How can I configure the registers of C6455 SRIO(especially the LSU_REG0~5 registers) for that the HOST device can visit the SLAVE one's CAR and CSR registers by means of Maintenance read/Maintenance write operation .
2. In a SRIO system, there are one C6455 devices as SRIO host device and a SWITCH device as slave device. This two devices connect directly through SRIO BUS.How can I configure the registers(especially the LSU_REG0~5 registers) of C6455 SRIO for that the HOST device can visit the SWITCH CAR registers by means of Maintenance read/Maintenance write operation .
Thanks