I am trying to enable EDMA region 1 by writing in the DRAE1 register located at the address 0x01C00000+0x340+0x8, the value I am writing is 0xFFFFFFFF and when I read it back I get 0x0. I did the same with DRAE0 and the value I read back is correct (0xFFFFFFFF). Is there anything else I need to do before I enable DRAE1 ? I am referring to OMAP-L138.pdf & omap-l138.pdf.
I printed the Revision ID Register (REVID) which is 0x40019b00 and also the EDMA3CC Configuration Register (CCCFG) which is 0x213344 for EDMA_3_0 but 0x203344 for EDMA_3_1. My datasheet has the value R-4001 5300h for REVID register and looking at the CCCFG register the values appear incorrect.