Hello, I want to compare the actual speed of the edma3 and it's theory value, my platform is based on tms320c6455,
the core frequence is 1GHz, and I use edma3 transfer data from DDR2 to DDR2, I found that the edma3 clock is sys_clk2, whose frequence is
fixed at CPU/3,so it's clock peorid is 3ns, and DDR2's clock is 250MHz, but DDR2 can transfer data on both edge of the clock ,so it's actual frequence is 500MHz
, so ,I thougnt that the speed is limited by the edma3 clock,but I'm not sure the bus width of edma3,I think it is also related with SCR, and I confused , how can I compute the transfer speed of edma3,can someone help me.