Other Parts Discussed in Thread: DA8XX
Hello,
My customer is saying that some spike noise was seen on DVDD pins, especially on E12,F12,G12 and F11 with their target board. In fact, these pins are present beside EMIFB pins so they are wondering if the noise might come from EMIFB. And they are also saying the noise can be routed to McASP data lines. I saw some captures on the McASP data line with the spike noise and found the similar noise appeared in both pins . Please take a look :
Now If they apply 1000pF and 0.1uF bypass capacitors, the noise seems to be reduced considerably.
So they questions are
1. Can you suggest which DVDD pin is related to each peripheral ? It seems they want to know the exact power network inside the device and apply their workaround for exact pins. Is it possible for you to share such information ?
2. Do you have any guide line for noise immunity ? I think we can suggest the following wiki for bypass capacitors, but do you have any other references for robust design for the noise ?
Best Regards,
Naoki
===
PS :The device is actually not C6747, but DA8xx.