Tool/software: TI-RTOS
Hi,
I am using the VoLib CID component to implement the caller ID for British Telecom standard. According to the VoLib documentation, it should be supported.
- BT SIN 227, CDS Calling Line Identification Service
- BT SIN 242, CDS Calling Line Identification Service
It works well in most of the cases. However, the experimental result finds out the Channel Seizure time has to be >170ms which is too long..
According to the BT spec., it should be (80 ms < Channel Seizure Duration < 262 ms)
In order to recognize British Telecom CID, in the cidCtlMsg, the ctlCode = cid_CTL_DTCT_BT and leading_marks = 0.
Do you know if there is other parameter that I can configure the Channel Seizure time for CID detector?
Thanks,