hi,
i have a dought that how to read a data during runing of dsp 6713 .Weather to use scanf or there is another key word
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
i have a dought that how to read a data during runing of dsp 6713 .Weather to use scanf or there is another key word
hi
I am doing one project which is on dsp 6713 .The project is voice based calculations suppose when i say 2*2 to the system it must say 4 to me
to do this please send your valuable information fior this project
What platform are you using with the TMS320C6713? Is it your own target hardware, or the DSK from Spectrum Digital?
Secondly, what does your development platform look like?
How are you wanting to interface to the TMS320C6713?
There are many DSP/BIOS examples that target the DSK6713 from Spectrum Digital.
Spectrum Digital's Support site for the DSK6713 is found at http://c6000.spectrumdigital.com/dsk6713/.
Actually iam doing a project based on voice processing. the theme of project is based on voice it has to do calculations ,means when i say 2+2 it must reconige it and give reply as 4 in voice to do this please give ur valuable information. Iam doing on ccstudio the platform is 'c'
Actually iam doing a project based on voice processing. the theme of project is based on voice it has to do calculations ,means when i say 2+2 it must reconige it and give reply as 4 in voice to do this please give ur valuable information. Iam doing on ccstudio the platform is 'c' on dsp6713
Actually iam doing a project based on voice processing. the theme of project is based on voice it has to do calculations ,means when i say 2+2 it must reconige it and give reply as 4 in voice to do this please give ur valuable information. Iam doing on ccstudio the platform is 'c' which is on dsp 6713
Please do not make the same post repeatedly in multiple threads under multiple titles, I combined them all into this thread for now.
As to the question at hand you will need to do some searching around for voice recognition algorithms and implement them on your 6713 (we have some third party companies who make such algorithms), we can help with issues you come across doing so, but your question at this point is a bit too broad.
Hi,
Please create your new request as a new thread, so that, we could better address your query compared to following up on old thread.
Thanks for your understanding.
Regards,
Sivaraj K