Dear Sir:
I try to use C6748 SATA interface to access SATA hard disk. The related software version I use are:
CCSV3.3
DSP/BIOS 5.41.10.36
edma3_lld_01_11_00_02
rtfs_1_10_02_32
pspdrivers_01_30_01
biosusb_01_10_03
The target board I use is our own design. When I run C6748 experimenter test program, the response is:
-> Attempting to spin up SATA disk...
-> ...disk spin-up success.
Which means the SATA interface works. But when I run RTFS sata example program, the response is:
ATA Hard Drive Application Task 0 Starting.
Configured ATA drive.
Version : 0001.0100
NumOfCmdSlots : 32
NumOfPorts : 1
Speed : 3 Gbps
SATA:AHCI-CAP:SNCQ SSNTF SMPS SSS SLAP SAL SCLO SAM SPM PMD SSC PSC
Block Driver Initialization Succeeded
ATA Build: Debug.
SATA PHY Not initialized : offline
Check for SATA cable connected properly
I have read all related POSTs and try the method they pointed to, but I still could not get it done.
Did I miss some steps to setup? Could someone help me out?
Thank you so much.
Yu-Fu