Hi everyone. i have a problem with dsk c6713. i have already installed ccs v3.1 & dsk6713 drivers and target content. when i try to run 6713 dsk diagnostic, a warning is appearing as below.
Can anyone suggest to me how to solve this problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone. i have a problem with dsk c6713. i have already installed ccs v3.1 & dsk6713 drivers and target content. when i try to run 6713 dsk diagnostic, a warning is appearing as below.
Can anyone suggest to me how to solve this problem?
Hi,
Thanks for your post.
I think, drivers for the peripherals (board support libraries), gel files and board specific content files would be missing. Usually, the Board Support Library comes from the board vendor and in your case, it would be Spectrum Digital. Please download the Target Content (.zip) file from the link given below.
http://c6000.spectrumdigital.com/dsk6713/
If you are using the on-board emulator and running the DSK Diagnostics utility at the same time as CCS, please try shutting down CCS and then running the diagnostic again.
Also, I would suggest running Spectrum Digital's SDConfig utility first to check the JTAG connection at a lower level.
Please see this troubleshooting page that covers the SDConfig usage: http://support.spectrumdigital.com/guides/JTAG_Emulator_guide/
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------
Hai.
Thanks for your reply. I already download the Target Content (.zip) file from the link given. But i do not know what to do with them. Can u please give me some more details? Sorry because i am new to this device.
And may i ask about the second link given about JTAG Emulator.Do i need the JTAG Emulator to run this dsk6713? im a bit confuse here. Thanks.
Hi Sivaraj
Now i already can run the 6713 dsk diagnostic. But now i have new problem. I try to start the diagnostic test but it is failed as the screenshot below.
Is it because of the usb connection? But the device manager already detect the tms320c6713 dsk.
Can u suggest to me what is the reason for this problem? Thanks
Hi,
Thanks for your update.
I think, the below E2E post would help you to understand USB diagnostic failure in c6713 dsk. Please go through the referred post as follows:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/182711.aspx
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------