Hi,
I should use eMMC V4.4 (and V4.3) compliant chip in my c6745 design. c6745 seems to be V4.0 compliant. Is this interface operational, I don't need boot -properties, just data R/W with my application, booted from EEPROM.
Risto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I should use eMMC V4.4 (and V4.3) compliant chip in my c6745 design. c6745 seems to be V4.0 compliant. Is this interface operational, I don't need boot -properties, just data R/W with my application, booted from EEPROM.
Risto
Hi Risto,
http://processors.wiki.ti.com/index.php/Managed_NAND
C6745 would support eMMC with V4.0 compliant,
It is operational and tested with eMMC compliant V4.0,
but, I'm not sure for v4.4 or v4.3
Hello Hedman,
Yes. the C6745 device is compliant to MMC V4.0 (Not V4.3 or V4.4), which means it can support MMC 8 bit mode at 52 MHz.
If you don't need any boot features supported by V4.3 or V4.4 and just doing data R/W, i would recommend you to use V4.0 chip instead going with higher version chip with additional cost..
Regards,
Senthil
Thank you Senthil,
Does this V4.0 interface allow card capacities up to 32G?
Best Regards,
Risto
Hi Risto
As per the MMC v4.0 specs the support for 32 GB came out on later versions and is not part of v4.0 spec.
The MMC/SD controller on C6745 is same as what we have on other devices within the ARM+DSP, DSP only, ARM only family (OMAPL138, OMAPL137, C6748, AM18xx, AM17xx)
So you might find some of the following threads useful
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/290019.aspx
We have tested with 32GB SDHC , but I do not believe we have done any testing with higher density MMC/eMMC.
Please also note that c6745/OMAPL137/AM17 does not support booting from MMC/SD , OMAPL138/C6748/AM8xx does.
Regards
Mukul
Thank you Mukul,
So if you have tested 32GB SDHC there should not be HW- interface problem. I'm actually using "Managed NAND" Titus referenced in his reply. Are there any app. note, code or other additional information about your 32GB SDHC test - 32G is my target density.
risto
Hi Risto
I have not looked at the subtle differences in the SD vs MMC specs. SDHC would be governed by the SD spec, and we do show in the datasheet that SDHC is supported.
Managed nand, these days is typically eMMC, and I am not aware of us testing any MMC or eMMC with 32 GB density. I am not sure if it works, so I recommend testing this out as part of your evaluation before making final design decision.
Regards
Mukul