Does the C6748 support USB 2.0 test modes? There is a USBHSET utility available from USB.org that configures USB devices for compliance testing. Does the C6748's USB interface work with USBHSET?
Thanks,
Tobyn
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does the C6748 support USB 2.0 test modes? There is a USBHSET utility available from USB.org that configures USB devices for compliance testing. Does the C6748's USB interface work with USBHSET?
Thanks,
Tobyn
Hello Tobyn,
Yes, the C6748 device supports USB 2.0 compliance testing.
USBHSET shall be used as an electrical test utility for C6748 USB 2.0 upstream device compliance testing, but it is not applicable for downstream host compliance testing (Refer Section 3: Required Instruments in below links).
Please refer below links for more details about C6748 USB 2.0 compliance testing.
http://www.ti.com/lit/an/sprab51/sprab51.pdf
http://www.ti.com/lit/an/sprab50/sprab50.pdf
Regards,
Senthil