Hello,
I'm using UPP on a C6748 facing a FPGA.
The FPGA is sending Burst of data to DSP. The frequency of the UPP is 50 Mhz. The size of the data burst is 72 bytes.
I'm queueing 2 DMAs with 72 bytes each on my DSP, I receive the 1rst burst from the FPGA but I noticed that if the FPGA is sending the 2nd burst very closed to the second one (1 CLCK) , that is to say : the Start signal of the 2 nd burst is 20 ns after the end of the last data of the 1st burst then the 2nd burst is lost, I have no interrupt for it.
Could you tell me if the UPP component need a certain delay for switching betwen 2 DMAs ?
Thank you very much for your help.
regards,
Pat