Hi.
One of my customers reported that the C6746 PINMUX10_3_0 field of the PINMUX10 register is set to 1h, which is undefined value, at the NOR boot. Since the customer uses the pin for GPIO, he would like to know the input/output type of the undefind setting. His concern is output conflict of the pin. Would you please tell me the input/output type of the PINMUX10_3_0 setting?
You can also know that PINMUX10_3_0 is set to 1 at the following E2E post:
https://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/43029/150324#150324
It seems that the ROM bootloader sets PINMUX10_3_0 for EMA_A[23], but the number of the EMIFA address lines is 23.
Best regards,
Tsutomu Furuse