Hi,
I'm trying to deploy the uPP BIOS driver which is supplied with PSP 1.30.1 for C6748.
My first step was to try and run the example given with the same PSP (simple loop-back between the two channels), it fails.
The loop-back transmit/receive sequential pattern.
If I try the loop-back at 8-bit width, 75MHz (the given example without any change), it misses every third byte.
If I try my own configuration (16-bit, 50MHz) I get the following pattern -
00 01 02 01 06 05 08 09 0C 0D 0E 0D 12 11 14 15 18 19 1A 19 1C 1D 1E 1D 22 21
24 25 28 29 2A 29 2E 2D 30 31 34 35 36 35 3A 39 3C 3D 40 41 42 41 46 45 48 49
4C 4D 4E 4D 52 51 54 55 58 59 5A 59 5E 5D 60 61 64 65 66 65 6A 69 6C 6D 70 71
72 71 76 75 78 79 7C 7D 7E 7D 80 81 82 81 86 85 88 89 8C 8D 8E 8D 92 91 94 95
98 99 9A 99 9E 9D A0 A1 A4 A5 A6 A5 AA A9 AC AD B0 B1 B2 B1 B6 B5 B8 B9 BC BD
BE BD C2 C1 C4 C5 C8 C9 CA C9 CE CD D0 D1 D4 D5 D6 D5 DA D9 DC DD E0 E1 E2 E1
E4 E5 E6 E5 EA E9 EC ED F0 F1 F2 F1 F6 F5 F8 F9 FC FD FE FD 02 01 04 05 08 09
0A 09 0E 0D 10 11 14 15 16 15 1A 19 1C 1D 20 21 22 21 ..........................
Any idea?
Regards,
Uri