Hi,
I'm trying to use C6747 cycle accurate simulator, and I have a question about simulator in CCSv5.
I created a typical sys/bios project and built the project successfully. When I see the memory map, all the program seem to be located in the section starts from 0xC0000000, SDRAM section. I wonder if this memory allocation would affect the performance or not. I saw other post in E2E which says that the cycle accurate simulator doesn't emulate cache, so I imagine that the memory allocation will not affect the performance.
Or if the memory allocation affects the performance, how can I change the memory allocation?
I tried to change it at .cfg file, but when I change it, I couldn't start the debugger correctly and I couldn't entry to main() function.
Thank you in advance.
Shintaro