Tool/software: Starterware
I am currently trying to use multiple interrupts(int4 through int15). With all these interrupts registered correctly, how do I control each of interrupts' priority? Does the priority of interrupt goes by INT# such as INT4, INT5, INT6, ... , INT15? or do I need to write specific code to register the priority of each interrupt?
For the second issue, in starterware SPI driver, which is SPI.C, it seems to me that SPI tx and rx interrupt are mapped to INT1. and on the datasheet too. does this INT1 mean INTERRUPT #1? Isn't there any way I can map this to other location like INT8 or somewhere between INT4 and INT15?