Other Parts Discussed in Thread: TMS320C6748, SYSBIOS
Tool/software: TI-RTOS
Hi all,
I have to apply my graduation project on a development kit. After search on TI’s site, I found that TMDSLCDK6748 is a suitable kit for me.
But it does not have an on-board emulator, as said on the official site "The LCDK does not have an onboard emulator. An external emulator from TI or a third-party will be required to start development".
So, what is the appropriate emulator that can be installed on the kit and connected to its pins without no problems?
I found that one "XDS100v2 JTAG Debug Probe 14-pin TI version",
www.ti.com/.../TMDSEMU100V2U-14T
but i do not know if can be suitable or not, what about the probe number of pins and other ones on the kit? are they compatible?
Also, the kit uses DSP/BIOS as the main operating system as mentioned in its features; I want to use TI/RTOS or SYS/BIOS, is this possible?
On the site, I found here in link below that SYS/BIOS can support "TMS320C6748", is that ok? or is there any other suitable probe for the kit ?
www.ti.com/.../biossw-c6748
Thanks in advance.