Hi,
I am trying to use fastboot (on a 32bit Windows7) to update the EMMC firmware but fastboot is not seeing my device.
I have installed fastboot on the pc and have also installed the driver for the AM335xevm. The Device Manager properties showed "this device is working properly"
with USB\VID: USB\VID_0451&PID_D022
Device Manager showed:
Universal Serial Bus devices
AM335xevm
On power-up, I hit "enter" a few times and was able to get into "U-Boot#", I then typed in "fastboot" and got
mmc_send_cmd : timeout: No status update
mmc1(part 0) is current device
mmc_send_cmd : timeout: No status update
Loading efi partition table:
256 128k spl
512 512k blootloader
and so on,,,,,
Fastboot entered .....
musb-hdrc: peripheral reset irq lost!
Then, on a different command window where abd.exe and fastboot.exe are located, I typed "fastboot devices" and got nothing.
I have also tried "fastboot oem format" and got < waiting for devices >
When the device is NOT in "fastboot" mode, adb is working fine, I can issue "adb devices" and get:
0123456789ABCDEF devices
Thank you in advance for your help.