Hi
I wanna change screen resolution 800x480 or similer value.
How can i change screen resolution Android 4.2.2 KitKat on Beaglebone black?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I wanna change screen resolution 800x480 or similer value.
How can i change screen resolution Android 4.2.2 KitKat on Beaglebone black?
Hello,
You don't need to flash the BBB_JB_Android_3_8_13.img, the image from TI_Android_JB_4.2.2_Devkit works fine.
Once you flashed the TI_Android_JB_4.2.2_Devkit image, you will have 4 partitions on your SD card.
One of them will contains those files: uImage, uEnv.txt, u-boot.img, MLO, ...
uEnv.txt contains some variables that u-boot (the bootloader) will read before starting the kernel.
You want to open this file, and append to the 'bootargs' variable's line the resolution you want.
This is the line by default:
bootargs=console=ttyO0,115200n8 androidboot.console=ttyO0 mem=512M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
This is an example of what you want:
bootargs=console=ttyO0,115200n8 androidboot.console=ttyO0 mem=512M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off video=1280x720-16@60