Hello all,
I use u-boot-2013.01.01-psp06.00.00.00 and linux-3.2.0-psp04.06.00.11 with an AM3356 processor for a custom board.
In the U-Boot code, I make the initialization of the pin "mcasp0" for an external component.
Then U-Boot launch the linux kernel which initialize the "mcasp0" pin before entering into the "am335x_evm_init(void)" function in "arch/arm/mach-omap2/board-am335xevm.c" file.
Do you know where is this kernel IO reset ?
I tried to stop this initialization by modifying functions in "arch/arm/mach-omap2/omap_hwmod.c" but without success.
If you have any ideas, your welcome. Thanks.