Hi,
I am facing the Linux kernel booting issue in AM335 customized board.
Please see the below Customize board log:
U-Boot SPL 2011.09 (Jun 20 2014 - 14:52:20)
Texas Instruments Revision detection unimplemented
### Use AM335x_SK V1.2 setting ###
No daughter card present
boot_device=8
OMAP_HSMMC1_BASE 1
OMAP SD/MMC: 0
boot mode - FAT
reading u-boot.img
spl_parse_image_header inside if
reading u-boot.img
U-Boot 2011.09 (Jun 20 2014 - 14:52:20)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
### Use AM335x_SK V1.2 setting ###
No daughter card present
NAND: HW ECC Hamming Code selected
No NAND device found!!!
0 MiB
MMC: omap_mmc_init dev_index = 0
OMAP_HSMMC1_BASE 1
OMAP SD/MMC: 0
*** Warning - readenv() failed, using default environment
Net: cpsw
Hit any key to stop autoboot: 0
SD/MMC found on device 0
reading uEnv.txt
** Unable to read "uEnv.txt" from mmc 0:1 **
reading uImage
2591448 bytes read
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2591384 Bytes = 2.5 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@localhost) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #3 Mon Jun 30 10:58:28 IST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 254464k/254464k available, 7680k reserved, 0K highmem
[ 0.000000] ankur 1 Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0492000 (4648 kB)
[ 0.000000] .init : 0xc0492000 - 0xc04ca000 ( 224 kB)
[ 0.000000] .data : 0xc04ca000 - 0xc051a290 ( 321 kB)
[ 0.000000] .bss : 0xc051a2b4 - 0xc0543804 ( 166 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000122] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.058532] pid_max: default: 32768 minimum: 301
[ 0.058685] Security Framework initialized
[ 0.058776] Mount-cache hash table entries: 512
[ 0.059143] CPU: Testing write buffer coherency: ok
[ 0.079040] omap_hwmod: pruss: failed to hardreset
[ 0.080139] print_constraints: dummy:
[ 0.080505] NET: Registered protocol family 16
[ 0.082611] OMAP GPIO hardware version 0.1
[ 0.084747] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.086914] omap_i2c.1: alias fck already exists
[ 0.088256] edma.0: alias fck already exists
[ 0.088287] edma.0: alias fck already exists
[ 0.088287] edma.0: alias fck already exists
[ 0.106231] bio: create slab <bio-0> at 0
[ 0.108123] SCSI subsystem initialized
[ 0.128601] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.130493] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.132873] print_constraints: VRTC:
[ 0.134307] print_constraints: VIO: at 1500 mV
[ 0.136596] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.138885] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.139892] print_constraints: VDD3: 5000 mV
[ 0.141296] print_constraints: VDIG1: at 1800 mV
[ 0.142730] print_constraints: VDIG2: at 1800 mV
[ 0.144134] print_constraints: VPLL: at 1800 mV
[ 0.145568] print_constraints: VDAC: at 1800 mV
[ 0.146972] print_constraints: VAUX1: at 1800 mV
[ 0.148376] print_constraints: VAUX2: at 3300 mV
[ 0.149841] print_constraints: VAUX33: at 3300 mV
[ 0.151245] print_constraints: VMMC: at 3300 mV
[ 0.151733] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.153869] Switching to clocksource gp timer
[ 0.169433] NET: Registered protocol family 2
[ 0.169647] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.169952] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.170104] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.170196] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.170196] TCP reno registered
[ 0.170227] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.170257] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.170410] NET: Registered protocol family 1
[ 0.170684] RPC: Registered named UNIX socket transport module.
[ 0.170715] RPC: Registered udp transport module.
[ 0.170715] RPC: Registered tcp transport module.
[ 0.170715] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.170959] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.182403] VFS: Disk quotas dquot_6.5.2
[ 0.182495] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.183013] msgmni has been set to 497
[ 0.186187] alg: No test for stdrng (krng)
[ 0.186859] io scheduler noop registered
[ 0.186889] io scheduler deadline registered
[ 0.186950] io scheduler cfq registered (default)
[ 0.188110] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.661071] console [ttyO0] enabled
[ 0.665313] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.673126] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.680908] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.688659] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.696411] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.713287] brd: module loaded
[ 0.721405] loop: module loaded
[ 0.724914] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.731384] i2c-core: driver [tsl2550] using legacy resume method
[ 0.737823] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.804229] No daughter card found
[ 0.807830] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.822998] Board name: A335X_SK
[ 0.826385] Board version: 1.2B
[ 0.829650] The board is a AM335x Starter Kit.
[ 0.834503] omap_hsmmc.0: alias fck already exists
[ 0.841491] registered am33xx_sr device
[ 0.847045] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 0.854980] CAN device driver interface
[ 0.858978] CAN bus driver for Bosch D_CAN controller 1.0
[ 0.914306] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 0.920745] davinci_mdio davinci_mdio.0: detected phy mask fffffffc
[ 0.928863] davinci_mdio.0: probed
[ 0.932434] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 0.939819] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 0.947723] mousedev: PS/2 mouse device common for all mice
[ 0.954559] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[ 0.961212] omap_rtc: already running
[ 0.965209] i2c /dev entries driver
[ 0.971191] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 0.979705] cpuidle: using governor ladder
[ 0.984497] cpuidle: using governor menu
[ 0.991760] omap4_aes_mod_init: loading AM33X AES driver
[ 0.997467] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.003967] omap4_aes_probe: probe() done
[ 1.008636] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.014770] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.024383] mmc_wait_for_cmd : cmd->opcode = 52
[ 1.029937] mmc_app_cmd : mmc_wait_for_req err = -110
[ 1.035491] mmc_wait_for_cmd : cmd->opcode = 52
[ 1.041107] mmc_app_cmd : mmc_wait_for_req err = -110
[ 1.047882] mmc_wait_for_cmd : cmd->opcode = 0
[ 1.053619] omap4_sham_probe: probe() done
[ 1.058074] mmc_app_cmd : mmc_wait_for_req err = 0
[ 1.064666] oprofile: hardware counters not available
[ 1.069915] oprofile: using timer interrupt.
[ 1.074432] nf_conntrack version 0.5.0 (3976 buckets, 15904 max)
[ 1.081146] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.086822] TCP cubic registered
[ 1.090209] NET: Registered protocol family 17
[ 1.094848] can: controller area network core (rev 20090105 abi 8)
[ 1.101379] NET: Registered protocol family 29
[ 1.106048] can: raw protocol (rev 20090105)
[ 1.110504] can: broadcast manager protocol (rev 20090105 t)
[ 1.116455] Registering the dns_resolver key type
[ 1.121398] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.129425] ThumbEE CPU extension supported.
[ 1.133941] mux: Failed to setup hwmod io irq -22
[ 1.139465] Power Management for AM33XX family
[ 1.144287] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.150970] Copied the M3 firmware to UMEM
[ 1.155426] Compensating OPP0 for 0mV Orig nvalue:0x99c3b2 New nvalue:0x99c3b2
[ 1.163055] Compensating OPP1 for 0mV Orig nvalue:0x998e80 New nvalue:0x998e80
[ 1.188049] Compensating OPP0 for 0mV Orig nvalue:0x99bbae New nvalue:0x99bbae
[ 1.195709] Compensating OPP1 for 0mV Orig nvalue:0x999b8c New nvalue:0x999b8c
[ 1.203308] Compensating OPP2 for 0mV Orig nvalue:0xaae6d1 New nvalue:0xaae6d1
[ 1.210968] Compensating OPP3 for 0mV Orig nvalue:0xaacbb8 New nvalue:0xaacbb8
[ 1.218658] create_regulator: VDD1: Failed to create debugfs directory
[ 1.378814] Detected MACID=1c:ba:8c:e8:66:a7
[ 1.384246] cpsw: Detected MACID = 1c:ba:8c:e8:66:a9
[ 1.390502] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:26:45 UTC (946686405)
[ 1.399688] Waiting for root device /dev/mmcblk0p2...
[ 1.546447] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.632690] mmc0: new high speed SDHC card at address aaaa
[ 1.639678] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[ 1.646118] mmcblk0: p1 p2 p3
[ 1.747985] kjournald starting. Commit interval 5 seconds
[ 1.753753] EXT3-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
[ 1.779205] mmc_wait_for_cmd : cmd->opcode = 13
[ 1.784210] mmc_app_cmd : mmc_wait_for_req err = 0
[ 1.789520] EXT3-fs (mmcblk0p2): using internal journal
[ 1.794982] EXT3-fs (mmcblk0p2): recovery complete
[ 1.799987] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 1.807220] VFS: Mounted root (ext3 filesystem) on device 179:2.
[ 1.813812] Freeing init memory: 224K
[ 1.849029] Unable to handle kernel paging request at virtual address fffffffc
[ 1.857299] pgd = c0004000
[ 1.860107] [fffffffc] *pgd=8fffe821, *pte=00000000, *ppte=00000000
[ 1.866668] Internal error: Oops: 17 [#1]
[ 1.870849] Modules linked in:
[ 1.874023] CPU: 0 Not tainted (3.2.0 #3)
[ 1.878601] PC is at kthread_data+0x10/0x18
[ 1.882965] LR is at wq_worker_waking_up+0x14/0x54
[ 1.887969] pc : [<c00560cc>] lr : [<c005214c>] psr: 60000193
[ 1.887969] sp : cfa25d08 ip : cfa25d18 fp : cfa25d14
[ 1.899932] r10: 00000003 r9 : cfa25df0 r8 : 00000000
[ 1.905395] r7 : c0744200 r6 : 00000000 r5 : 60000193 r4 : 00000000
[ 1.912200] r3 : 00000000 r2 : 00000001 r1 : 00000000 r0 : cf81bc00
[ 1.919006] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 1.926696] Control: 10c5387d Table: 8fa70019 DAC: 00000015
[ 1.932708] Process mmcqd/0 (pid: 678, stack limit = 0xcfa242f0)
[ 1.938964] Stack: (0xcfa25d08 to 0xcfa26000)
[ 1.943511] 5d00: cfa25d2c cfa25d18 c005214c c00560c8 00400100 cf81bc00
[ 1.952056] 5d20: cfa25d4c cfa25d30 c0038868 c0052144 cfa25df0 cf81dd44 00000000 00020028
[ 1.960571] 5d40: cfa25d5c cfa25d50 c0038880 c00387bc cfa25d74 cfa25d60 c00564ac c0038878
[ 1.969116] 5d60: cfa25df0 c07438e0 cfa25d94 cfa25d78 c005653c c00564a4 cfa25df0 c07441f4
[ 1.977661] 5d80: c00564d4 00000001 cfa25dcc cfa25d98 c0037478 c00564e0 cfa25dbc 00000001
[ 1.986175] 5da0: c00733f8 20000193 cf8856c0 00000001 cf8856c0 cfa21000 cf8856c0 00000000
[ 1.994720] 5dc0: cfa25dec cfa25dd0 c00374e0 c003742c cfa25df0 00000004 fa200000 000002d8
[ 2.003265] 5de0: cfa25e04 cfa25df0 c0056468 c00374c4 c07438e0 00000000 cfa25e1c cfa25e08
[ 2.011779] 5e00: c007ab78 c0056440 20000193 cfa68b30 cfa25e3c cfa25e20 c00d9808 c007ab18
[ 2.020324] 5e20: c00d9798 cf8856c0 cfa2d8f8 00000000 cfa25e4c cfa25e40 c00d1ce0 c00d97a4
[ 2.028839] 5e40: cfa25e6c cfa25e50 c01bb1c4 c00d1cb0 00000000 00010000 00010000 00010000
[ 2.037384] 5e60: cfa25eac cfa25e70 c01bb318 c01bb148 cfa40000 00010000 cfa2d8d8 00000000
[ 2.045928] 5e80: cfa25ed4 cfa2d8d8 00000000 00000000 cfa21028 cfa21000 cfa2d9b0 00000000
[ 2.054443] 5ea0: cfa25ecc cfa25eb0 c01bb664 c01bb224 00000000 00000000 cfa2d8d8 cfa21004
[ 2.062988] 5ec0: cfa25eec cfa25ed0 c01bbb90 c01bb654 00000000 cfa2d8d8 cfa21400 cfa21004
[ 2.071533] 5ee0: cfa25efc cfa25ef0 c01bbdf4 c01bbb84 cfa25f44 cfa25f00 c0293634 c01bbdec
[ 2.080047] 5f00: cfa25f54 00000000 cfa2123c 00000001 cfa21400 00000000 cfa24000 cfa21400
[ 2.088592] 5f20: cfa21004 cfa24000 cfa21000 cfa2d9b0 00000000 cfa21000 cfa25f8c cfa25f48
[ 2.097137] 5f40: c0293868 c029338c 00000000 cfa2d9b0 cfa25f74 cfa25f60 c01bbb74 c01bfc8c
[ 2.105651] 5f60: cfa2d9b0 cfa21004 00000000 cfa24000 00000001 cf99e730 00000000 cfa2100c
[ 2.114196] 5f80: cfa25fbc cfa25f90 c0294038 c02936dc 00000000 cf835cb0 cfa21004 c0293fdc
[ 2.122741] 5fa0: 00000013 00000000 00000000 00000000 cfa25ff4 cfa25fc0 c0055f7c c0293fe8
[ 2.131256] 5fc0: cf835cb0 00000000 cfa21004 00000000 cfa25fd0 cfa25fd0 00000000 cf835cb0
[ 2.139801] 5fe0: c0055eec c00406d8 00000000 cfa25ff8 c00406d8 c0055ef8 00000000 00000000
[ 2.148315] Backtrace:
[ 2.150878] [<c00560bc>] (kthread_data+0x0/0x18) from [<c005214c>] (wq_worker_waking_up+0x14/0x54)
[ 2.160247] [<c0052138>] (wq_worker_waking_up+0x0/0x54) from [<c0038868>] (try_to_wake_up+0xb8/0xbc)
[ 2.169769] r4:cf81bc00 r3:00400100
[ 2.173522] [<c00387b0>] (try_to_wake_up+0x0/0xbc) from [<c0038880>] (default_wake_function+0x14/0x18)
[ 2.183227] r6:00020028 r5:00000000 r4:cf81dd44 r3:cfa25df0
[ 2.189147] [<c003886c>] (default_wake_function+0x0/0x18) from [<c00564ac>] (autoremove_wake_function+0x14/0x3c)
[ 2.199768] [<c0056498>] (autoremove_wake_function+0x0/0x3c) from [<c005653c>] (wake_bit_function+0x68/0x6c)
[ 2.210021] r4:c07438e0 r3:cfa25df0
[ 2.213775] [<c00564d4>] (wake_bit_function+0x0/0x6c) from [<c0037478>] (__wake_up_common+0x58/0x98)
[ 2.223297] r6:00000001 r5:c00564d4 r4:c07441f4 r3:cfa25df0
[ 2.229217] [<c0037420>] (__wake_up_common+0x0/0x98) from [<c00374e0>] (__wake_up+0x28/0x34)
[ 2.238037] [<c00374b8>] (__wake_up+0x0/0x34) from [<c0056468>] (__wake_up_bit+0x34/0x3c)
[ 2.246551] r4:000002d8
[ 2.249206] [<c0056434>] (__wake_up_bit+0x0/0x3c) from [<c007ab78>] (unlock_page+0x6c/0x70)
[ 2.257934] [<c007ab0c>] (unlock_page+0x0/0x70) from [<c00d9808>] (mpage_end_io+0x70/0x108)
[ 2.266662] r4:cfa68b30 r3:20000193
[ 2.270385] [<c00d9798>] (mpage_end_io+0x0/0x108) from [<c00d1ce0>] (bio_endio+0x3c/0x5c)
[ 2.278930] r6:00000000 r5:cfa2d8f8 r4:cf8856c0 r3:c00d9798
[ 2.284851] [<c00d1ca4>] (bio_endio+0x0/0x5c) from [<c01bb1c4>] (req_bio_endio.clone.46+0x88/0xdc)
[ 2.294189] [<c01bb13c>] (req_bio_endio.clone.46+0x0/0xdc) from [<c01bb318>] (blk_update_request+0x100/0x430)
[ 2.304534] r6:00010000 r5:00010000 r4:00010000 r3:00000000
[ 2.310455] [<c01bb218>] (blk_update_request+0x0/0x430) from [<c01bb664>] (blk_update_bidi_request+0x1c/0x74)
[ 2.320831] [<c01bb648>] (blk_update_bidi_request+0x0/0x74) from [<c01bbb90>] (__blk_end_bidi_request+0x18/0x3c)
[ 2.331420] r6:cfa21004 r5:cfa2d8d8 r4:00000000 r3:00000000
[ 2.337341] [<c01bbb78>] (__blk_end_bidi_request+0x0/0x3c) from [<c01bbdf4>] (__blk_end_request+0x14/0x18)
[ 2.347412] r6:cfa21004 r5:cfa21400 r4:cfa2d8d8 r3:00000000
[ 2.353363] [<c01bbde0>] (__blk_end_request+0x0/0x18) from [<c0293634>] (mmc_blk_issue_rw_rq+0x2b4/0x350)
[ 2.363342] [<c0293380>] (mmc_blk_issue_rw_rq+0x0/0x350) from [<c0293868>] (mmc_blk_issue_rq+0x198/0x460)
[ 2.373352] [<c02936d0>] (mmc_blk_issue_rq+0x0/0x460) from [<c0294038>] (mmc_queue_thread+0x5c/0xf0)
[ 2.382873] [<c0293fdc>] (mmc_queue_thread+0x0/0xf0) from [<c0055f7c>] (kthread+0x90/0x94)
[ 2.391510] [<c0055eec>] (kthread+0x0/0x94) from [<c00406d8>] (do_exit+0x0/0x67c)
[ 2.399322] r6:c00406d8 r5:c0055eec r4:cf835cb0
[ 2.404144] Code: e1a0c00d e92dd800 e24cb004 e590312c (e5130004)
[ 2.410583] ---[ end trace f5d4b3f1c323f17f ]---
[ 2.415466] Unable to handle kernel NULL pointer dereference at virtual address 00000024
[ 2.424621] pgd = c0004000
[ 2.427459] [00000024] *pgd=00000000
[ 2.431182] Internal error: Oops: 17 [#2]
[ 2.435363] Modules linked in:
[ 2.438537] CPU: 0 Tainted: G D (3.2.0 #3)
[ 2.444091] PC is at wq_worker_waking_up+0x14/0x54
[ 2.449066] LR is at wq_worker_waking_up+0x14/0x54
[ 2.454071] pc : [<c005214c>] lr : [<c005214c>] psr: 60000193
[ 2.454071] sp : cfa25a20 ip : cfa25a20 fp : cfa25a34
[ 2.466064] r10: cf982f9c r9 : c04f86f8 r8 : cf982f9c
[ 2.471496] r7 : c04d09a0 r6 : 00000000 r5 : 20000193 r4 : 00000000
[ 2.478302] r3 : cf831fcc r2 : 00000001 r1 : 00000000 r0 : 00000000
[ 2.485107] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
[ 2.492645] Control: 10c5387d Table: 8fa70019 DAC: 00000015
[ 2.498626] Process mmcqd/0 (pid: 678, stack limit = 0xcfa242f0)
[ 2.504913] Stack: (0xcfa25a20 to 0xcfa26000)
[ 2.509460] 5a20: 84208040 cf81b680 cfa25a54 cfa25a38 c0038868 c0052144 00000001 20000193
[ 2.517974] 5a40: c04eab70 cfa24000 cfa25a64 cfa25a58 c003889c c00387bc cfa25a74 cfa25a68
[ 2.526519] 5a60: c0042648 c0038890 cfa25a8c cfa25a78 c0043030 c0042624 c04f7f68 60000113
[ 2.535064] 5a80: cfa25aa4 cfa25a90 c0075a3c c0042fe4 c04cc094 cf982ec0 cfa25ae4 cfa25aa8
[ 2.543579] 5aa0: c035efa8 c00759c0 ffffffff c035f3e0 c04d09a0 c04cc094 cfa25b7a cf982ec0
[ 2.552124] 5ac0: 00000001 cf982eb8 cf81bc00 cf982f9c cf982f9c cf982f9c cfa25af4 cfa25ae8
[ 2.560668] 5ae0: c035f3e0 c035ef64 cfa25b2c cfa25af8 c0040b40 c035f39c cfa24000 00000001
[ 2.569183] 5b00: cfa24000 cfa25b0c c00560d0 cfa25b0c cfa25b0c cf982fe4 c003d730 cfa25b7a
[ 2.577728] 5b20: cfa25bac cfa25b30 c0017c68 c00406e4 cfa242f0 0000000b 00000000 00000000
[ 2.586273] 5b40: 00000008 c0415a60 65000017 63306131 20643030 64323965 30303864 34326520
[ 2.594787] 5b60: 30306263 35652034 31333039 28206332 33313565 34303030 c0002029 c035eb5c
[ 2.603332] 5b80: c0431474 cfa25cc0 fffffffc 00000000 00000017 00000000 cfa25df0 cf982ec0
[ 2.611877] 5ba0: cfa25bd4 cfa25bb0 c001a2f4 c0017b4c cfa25cc0 00000000 cfa25cc0 fffffffc
[ 2.620391] 5bc0: 00000007 00000017 cfa25c0c cfa25bd8 c001a458 c001a284 cfa25bd8 cfa25bd8
[ 2.628936] 5be0: c052dd7c 00000017 fffffffc c04d04ac 00000007 cfa25cc0 cfa25df0 00000003
[ 2.637451] 5c00: cfa25cbc cfa25c10 c00083a4 c001a310 cfa25cb0 0000003c c04eb0c0 00000001
[ 2.645996] 5c20: c04eb194 0000000a c00714ac cfa24000 00000044 00000000 cfa25cb0 0000003c
[ 2.654541] 5c40: c04eb0c0 00000000 cfa25c6c cfa25c58 c0042f80 c003a7f8 c007333c c0505d04
[ 2.663055] 5c60: cfa25c8c cfa25c70 c04eab70 cf81bc00 0000ee6c 00000000 c04eab70 cf81bc00
[ 2.671600] 5c80: cf81bc38 cf81bc00 cf81bc30 c04eab70 c04eab70 c04eab70 cf982ec0 c00560cc
[ 2.680145] 5ca0: 60000193 ffffffff cfa25cf4 00000000 cfa25d14 cfa25cc0 c0013e58 c0008374
[ 2.688659] 5cc0: cf81bc00 00000000 00000001 00000000 00000000 60000193 00000000 c0744200
[ 2.697204] 5ce0: 00000000 cfa25df0 00000003 cfa25d14 cfa25d18 cfa25d08 c005214c c00560cc
[ 2.705749] 5d00: 60000193 ffffffff cfa25d2c cfa25d18 c005214c c00560c8 00400100 cf81bc00
[ 2.714263] 5d20: cfa25d4c cfa25d30 c0038868 c0052144 cfa25df0 cf81dd44 00000000 00020028
[ 2.722808] 5d40: cfa25d5c cfa25d50 c0038880 c00387bc cfa25d74 cfa25d60 c00564ac c0038878
[ 2.731323] 5d60: cfa25df0 c07438e0 cfa25d94 cfa25d78 c005653c c00564a4 cfa25df0 c07441f4
[ 2.739868] 5d80: c00564d4 00000001 cfa25dcc cfa25d98 c0037478 c00564e0 cfa25dbc 00000001
[ 2.748413] 5da0: c00733f8 20000193 cf8856c0 00000001 cf8856c0 cfa21000 cf8856c0 00000000
[ 2.756927] 5dc0: cfa25dec cfa25dd0 c00374e0 c003742c cfa25df0 00000004 fa200000 000002d8
[ 2.765472] 5de0: cfa25e04 cfa25df0 c0056468 c00374c4 c07438e0 00000000 cfa25e1c cfa25e08
[ 2.774017] 5e00: c007ab78 c0056440 20000193 cfa68b30 cfa25e3c cfa25e20 c00d9808 c007ab18
[ 2.782531] 5e20: c00d9798 cf8856c0 cfa2d8f8 00000000 cfa25e4c cfa25e40 c00d1ce0 c00d97a4
[ 2.791076] 5e40: cfa25e6c cfa25e50 c01bb1c4 c00d1cb0 00000000 00010000 00010000 00010000
[ 2.799621] 5e60: cfa25eac cfa25e70 c01bb318 c01bb148 cfa40000 00010000 cfa2d8d8 00000000
[ 2.808135] 5e80: cfa25ed4 cfa2d8d8 00000000 00000000 cfa21028 cfa21000 cfa2d9b0 00000000
[ 2.816680] 5ea0: cfa25ecc cfa25eb0 c01bb664 c01bb224 00000000 00000000 cfa2d8d8 cfa21004
[ 2.825225] 5ec0: cfa25eec cfa25ed0 c01bbb90 c01bb654 00000000 cfa2d8d8 cfa21400 cfa21004
[ 2.833740] 5ee0: cfa25efc cfa25ef0 c01bbdf4 c01bbb84 cfa25f44 cfa25f00 c0293634 c01bbdec
[ 2.842285] 5f00: cfa25f54 00000000 cfa2123c 00000001 cfa21400 00000000 cfa24000 cfa21400
[ 2.850799] 5f20: cfa21004 cfa24000 cfa21000 cfa2d9b0 00000000 cfa21000 cfa25f8c cfa25f48
[ 2.859344] 5f40: c0293868 c029338c 00000000 cfa2d9b0 cfa25f74 cfa25f60 c01bbb74 c01bfc8c
[ 2.867889] 5f60: cfa2d9b0 cfa21004 00000000 cfa24000 00000001 cf99e730 00000000 cfa2100c
[ 2.876434] 5f80: cfa25fbc cfa25f90 c0294038 c02936dc 00000000 cf835cb0 cfa21004 c0293fdc
[ 2.884948] 5fa0: 00000013 00000000 00000000 00000000 cfa25ff4 cfa25fc0 c0055f7c c0293fe8
[ 2.893493] 5fc0: cf835cb0 00000000 cfa21004 00000001 cfa25fd0 cfa25fd0 00000000 cf835cb0
[ 2.902008] 5fe0: c0055eec c00406d8 00000000 cfa25ff8 c00406d8 c0055ef8 00000000 00000000
[ 2.910552] Backtrace:
[ 2.913116] [<c0052138>] (wq_worker_waking_up+0x0/0x54) from [<c0038868>] (try_to_wake_up+0xb8/0xbc)
[ 2.922637] r4:cf81b680 r3:84208040
[ 2.926361] [<c00387b0>] (try_to_wake_up+0x0/0xbc) from [<c003889c>] (wake_up_process+0x18/0x1c)
[ 2.935546] r6:cfa24000 r5:c04eab70 r4:20000193 r3:00000001
[ 2.941467] [<c0038884>] (wake_up_process+0x0/0x1c) from [<c0042648>] (wakeup_softirqd+0x30/0x34)
[ 2.950714] [<c0042618>] (wakeup_softirqd+0x0/0x34) from [<c0043030>] (raise_softirq+0x58/0x60)
[ 2.959808] [<c0042fd8>] (raise_softirq+0x0/0x60) from [<c0075a3c>] (rcu_sched_qs+0x88/0x90)
[ 2.968597] r4:60000113 r3:c04f7f68
[ 2.972351] [<c00759b4>] (rcu_sched_qs+0x0/0x90) from [<c035efa8>] (__schedule+0x50/0x394)
[ 2.980957] r4:cf982ec0 r3:c04cc094
[ 2.984710] [<c035ef58>] (__schedule+0x0/0x394) from [<c035f3e0>] (schedule+0x50/0x68)
[ 2.992980] [<c035f390>] (schedule+0x0/0x68) from [<c0040b40>] (do_exit+0x468/0x67c)
[ 3.001068] [<c00406d8>] (do_exit+0x0/0x67c) from [<c0017c68>] (die+0x128/0x2d8)
[ 3.008758] r7:cfa25b7a
[ 3.011413] [<c0017b40>] (die+0x0/0x2d8) from [<c001a2f4>] (__do_kernel_fault+0x7c/0x8c)
[ 3.019866] [<c001a278>] (__do_kernel_fault+0x0/0x8c) from [<c001a458>] (do_page_fault+0x154/0x1f0)
[ 3.029296] r8:00000017 r7:00000007 r6:fffffffc r5:cfa25cc0 r4:00000000
[ 3.036132] r3:cfa25cc0
[ 3.038879] [<c001a304>] (do_page_fault+0x0/0x1f0) from [<c00083a4>] (do_DataAbort+0x3c/0xa0)
[ 3.047760] [<c0008368>] (do_DataAbort+0x0/0xa0) from [<c0013e58>] (__dabt_svc+0x38/0x60)
[ 3.056304] Exception stack(0xcfa25cc0 to 0xcfa25d08)
[ 3.061584] 5cc0: cf81bc00 00000000 00000001 00000000 00000000 60000193 00000000 c0744200
[ 3.070098] 5ce0: 00000000 cfa25df0 00000003 cfa25d14 cfa25d18 cfa25d08 c005214c c00560cc
[ 3.078643] 5d00: 60000193 ffffffff
[ 3.082275] r8:00000000 r7:cfa25cf4 r6:ffffffff r5:60000193 r4:c00560cc
[ 3.089294] [<c00560bc>] (kthread_data+0x0/0x18) from [<c005214c>] (wq_worker_waking_up+0x14/0x54)
[ 3.098632] [<c0052138>] (wq_worker_waking_up+0x0/0x54) from [<c0038868>] (try_to_wake_up+0xb8/0xbc)
[ 3.108154] r4:cf81bc00 r3:00400100
[ 3.111907] [<c00387b0>] (try_to_wake_up+0x0/0xbc) from [<c0038880>] (default_wake_function+0x14/0x18)
[ 3.121612] r6:00020028 r5:00000000 r4:cf81dd44 r3:cfa25df0
[ 3.127532] [<c003886c>] (default_wake_function+0x0/0x18) from [<c00564ac>] (autoremove_wake_function+0x14/0x3c)
[ 3.138153] [<c0056498>] (autoremove_wake_function+0x0/0x3c) from [<c005653c>] (wake_bit_function+0x68/0x6c)
[ 3.148406] r4:c07438e0 r3:cfa25df0
[ 3.152160] [<c00564d4>] (wake_bit_function+0x0/0x6c) from [<c0037478>] (__wake_up_common+0x58/0x98)
[ 3.161682] r6:00000001 r5:c00564d4 r4:c07441f4 r3:cfa25df0
[ 3.167602] [<c0037420>] (__wake_up_common+0x0/0x98) from [<c00374e0>] (__wake_up+0x28/0x34)
[ 3.176422] [<c00374b8>] (__wake_up+0x0/0x34) from [<c0056468>] (__wake_up_bit+0x34/0x3c)
[ 3.184936] r4:000002d8
[ 3.187591] [<c0056434>] (__wake_up_bit+0x0/0x3c) from [<c007ab78>] (unlock_page+0x6c/0x70)
[ 3.196319] [<c007ab0c>] (unlock_page+0x0/0x70) from [<c00d9808>] (mpage_end_io+0x70/0x108)
[ 3.205017] r4:cfa68b30 r3:20000193
[ 3.208770] [<c00d9798>] (mpage_end_io+0x0/0x108) from [<c00d1ce0>] (bio_endio+0x3c/0x5c)
[ 3.217285] r6:00000000 r5:cfa2d8f8 r4:cf8856c0 r3:c00d9798
[ 3.223205] [<c00d1ca4>] (bio_endio+0x0/0x5c) from [<c01bb1c4>] (req_bio_endio.clone.46+0x88/0xdc)
[ 3.232574] [<c01bb13c>] (req_bio_endio.clone.46+0x0/0xdc) from [<c01bb318>] (blk_update_request+0x100/0x430)
[ 3.242919] r6:00010000 r5:00010000 r4:00010000 r3:00000000
[ 3.248840] [<c01bb218>] (blk_update_request+0x0/0x430) from [<c01bb664>] (blk_update_bidi_request+0x1c/0x74)
[ 3.259185] [<c01bb648>] (blk_update_bidi_request+0x0/0x74) from [<c01bbb90>] (__blk_end_bidi_request+0x18/0x3c)
[ 3.269775] r6:cfa21004 r5:cfa2d8d8 r4:00000000 r3:00000000
[ 3.275726] [<c01bbb78>] (__blk_end_bidi_request+0x0/0x3c) from [<c01bbdf4>] (__blk_end_request+0x14/0x18)
[ 3.285766] r6:cfa21004 r5:cfa21400 r4:cfa2d8d8 r3:00000000
[ 3.291717] [<c01bbde0>] (__blk_end_request+0x0/0x18) from [<c0293634>] (mmc_blk_issue_rw_rq+0x2b4/0x350)
[ 3.301696] [<c0293380>] (mmc_blk_issue_rw_rq+0x0/0x350) from [<c0293868>] (mmc_blk_issue_rq+0x198/0x460)
[ 3.311676] [<c02936d0>] (mmc_blk_issue_rq+0x0/0x460) from [<c0294038>] (mmc_queue_thread+0x5c/0xf0)
[ 3.321228] [<c0293fdc>] (mmc_queue_thread+0x0/0xf0) from [<c0055f7c>] (kthread+0x90/0x94)
[ 3.329833] [<c0055eec>] (kthread+0x0/0x94) from [<c00406d8>] (do_exit+0x0/0x67c)
[ 3.337646] r6:c00406d8 r5:c0055eec r4:cf835cb0
[ 3.342468] Code: e92dd818 e24cb004 e1a04001 eb000fdb (e5903024)
[ 3.348876] ---[ end trace f5d4b3f1c323f180 ]---
[ 3.353698] Fixing recursive fault but reboot is needed!
[ 3.608917] Unable to handle kernel paging reauest at virtual address e9e39034
[ 3.617187] pgd = cfa70000
[ 3.620025] [e9e39034] *pgd=00000000
[ 3.623748] Internal error: Oops: 5 [#3]
[ 3.627838] Modules linked in:
[ 3.631011] CPU: 0 Tainted: G D (3.2.0 #3)
[ 3.636566] PC is at set_voltage+0x7c/0x19c
[ 3.640960] LR is at regulator_get_voltage+0x34/0x3c
[ 3.646118] pc : [<c0028f18>] lr : [<c01f142c>] psr: 20000113
[ 3.646148] sp : cf927f08 ip : 0012e1fc fp : cf97f4c
[ 3.658111] r10: 00000118 r9 : ffff769c r8 : c05154a8
[ 3.663543] r7 : 00000001 r6 : cf9ccc00 r5 : cf9ccd18 r4 : 00000001
[ 3.670379] r3 : 00000118 r2 : cf9ccd18 r1 : e9e39000 r0 : 0012e1fc
[ 3.677185] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 3.684814] Control: 10c5387d Table: 8fa70019 DAC: 00000015
[ 3.690795] Process kworker/0:1 (pid: 312, stack limit = 0xcf9262f0)
[ 3.697418] Stack: (0xcf927f08 to 0xcf928000)
[ 3.701965] 7f00: cf81bc00 cfa61e00 cf927f34 cf927f20 c005b148 000fad00
[ 3.710510] 7f20: cf8956c0 cf8b4300 cf814800 cf926000 00000000 c0028e9c cf9ccc34 cf814805
[ 3.719024] 7f40: cf927f84 cf927f50 c00500ec c0028ea8 c04ec5b0 cf8b4310 c052ce28 cf8b4300
[ 3.727569] 7f60: c04ec5b0 cf8b4310 c052ce28 cf926000 00000009 c04ec5ac cf927fbc cf927f88
[ 3.736114] 7f80: c0051f64 c004ffd4 cf8b4300 c0051e08 00000013 cf833ee0 cf8b4300 c0051e08
[ 3.744628] 7fa0: 00000013 00000000 00000000 00000000 cf927ff4 cf927fc0 c0055f7c c0051e14
[ 3.753173] 7fc0: cf833ee0 00000000 cf8b4300 00000000 cf927fd0 cf927fd0 00000000 cf(33ee0
[ 3.761718] 7fe0: c0055eec c00406d8 00000000 cf927ff8 c00406d8 c0055ef8 feffabef fddff6ff
[ 3.770233] Backtrace:
[ 3.772796] [<c0028e9c>] (set_voltage+0x0/0x19c) from [<%h>] (process_one_worct+0x124/0x384)
[ 3.781616] [<c004ffc8>] (process_one_worct+0x0/0x384) from [<%h>] (worker_thread+0x15c/0x330)
[ 3.790618] [<c0051e08>] (worker_thread+0x0/0x330) from [<%h>] (kthread+0x90/0x94)
[ 3.798522] [<c0055eec>] (kthread+0x0/0x94) from [<%h>] (sys_setitimer+0x0/0x67c)
[ 3.806335] cr6:c00406d8 cr5:c0055eec cr4:cf833ee0
[ 3.811431] Code: e0862003 e250c000 ba000031 e5921080 (e5919034)
[ 3.817810] ---[ end trace f5d4b3f1c323f181 ]---
Please help me to resolve this issue...
Thanks in advance..
Regards,
Ankur