Hi all,
About the steps of “boot Linux kernel on EVM6678L”
I summarized the boot steps according user guide:
1. install CCS
update GEL file
2. run script: ./bootblob all
3. power off
connect Linux host to EVM using XDS100
keep switch as table 'EVM667x Program_evm'
power on, init XDS100
run script <CCS_DIR>/..../dss.sh program_evm.js evm6678l-le "eeprome51, nand"
Question:
Q1. Is there some problem in the above steps?
Q2. In step 3, when run dss.sh script, using: program_evm.js evm6678l-le “eeprom51, nand”
Or using: program_evm.js evm6678l
Q3. In step 3, init XDS100, how can i know the init is ok? then run the dss script?
(in other words, after init XDS100, when I run the dss script)
Q4. After step 3,
the Linux kernel have been boot ok?
or the Linux kernel is just flashed into NAND, have not been boot?
If not been boot, how to boot?
Q5. When should change switch as table 'EVM667XL NAND BOOT' ?
Thank you ALL very much!
Best Regards
Jerry Yao