Hi,
I have got an issue with printing and not sure whats going on here and was wondering if anyone could shed some light on this.
In my defconfig file I have got the following enabled
CONFIG_DYNAMIC_DEBUG=y
CONFIG_DEBUG_LL=y
CONFIG_DEBUG_KERNEL=y
I have a board specific file in which on the top line I have got #define DEBUG define before #include files
My log level in prinkt.h is defined as
/* printk's without a loglevel use this.. */
#define DEFAULT_MESSAGE_LOGLEVEL 4 /* KERN_WARNING */
/* We show everything that is MORE important than this.. */
#define MINIMUM_CONSOLE_LOGLEVEL 1 /* Minimum loglevel we let people use */
#define DEFAULT_CONSOLE_LOGLEVEL 8 /* anything MORE serious than KERN_DEBUG */
When i print something in the board specific file using pr_debug nothing gets printed on terminal. I am not sure what I have done wrong here.
Would be great if anyone can help on this.
Regards
Ali