Hi,
I am working with rdk 3.8.0 . and I wanna change substream resolution to CIF , how should I do?
I tried to modify Multich_tristream_fullfeature.c as below
/* Second stream */
pCameraOutPrm = &pCameraInstPrm->outParams[1];
pCameraOutPrm->dataFormat = SYSTEM_DF_YUV420SP_UV;
pCameraOutPrm->scEnable = FALSE;
pCameraOutPrm->scOutWidth = 320;
pCameraOutPrm->scOutHeight = 120;
pCameraOutPrm->standard = SYSTEM_STD_CIF;
pCameraOutPrm->outQueId = 1;
But the serial port print:
[m3video] 6658: ENCODE: All CH Create ... DONE !!!
[m3vpss ] SD displayInstId = 2
[m3vpss ] 6674: Assertion @ Line: 848 in links_m3vpss/display/displayLink_drv.c: status == FVID2_SOK : failed !!!
[m3video] ENCLINK:HEAPID:0 USED:29688
[m3video] 6661: ENCODE: Create ... DONE !!!
then the process crash...
Can anybody tell me how should I do ?