Hi,
We have a product in which we need the support of FAT Write at U-Boot. My base SDK is GLSDK 6.04.00.02 for DRA7xx. I understand that this support is not enabled by default in U-boot code provided by default in this GLSDK. So, I have added the below line to enable the FAT Write Support in include/configs/dra7xx_evm.h
#define CONFIG_FAT_WRITE.
But on using the u-boot built after taiking in this change, I am not able to write to either SD Card/ eMMC Device.
When I execute the below command:
fatwrite mmc 1:1 0x83000000 boot_part.txt
I get the following error:
mmc_send_cmd: timedout waiting on cmd inhibit to clear
Can any one tell why this error is occuring or are there any fixes which can be taken, so that I do not see this issue?