HI all,
I am using our custom board based on am335x sk with SDK6. When running the video example scripts, such as runMpeg4AacDec.sh, it just lasts for a very short time(maybe 1 sec or less), then it halts and the system is stuck here. Using the "Ctrl + c" is not working at all. It is the same situation when manually run the video with "gst-launch-0.10 filesrc location=/usr/share/ti/video/HistoryOfTIAV-WVGA.mp4 ! qtdemux name=demux demux.au".
Here is the logs:
numid=1,iface=MIXER,name='PCM Playback Volume'
; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
: values=127,127
| dBscale-min=-63.50dB,step=0.50dB,mute=0
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstAudioSinkClock
Would anyone here can help me to solve this problem or give some other methods to play a video?
Thanks in advanced!!