Hi TI Experts,
I'm working customized DM385 platform.
I have 3 streams (From camera1 FULLHD and QVGA ) From camera2( D1 resolution )
Using streaming Application(wis-streamer ) I can able to see QVGA stream only...
Based on msg_type and video_type they are setting the streams and reading from the shared memory !!!
Can you tell me the flow to access the streams and where I can get the msg_type and video_type ??
Thanks & Regards,
Rajesh Kannan.S