Hi all,
I've been trying to run standalone application using Uboot in Beaglebone black but unable to do so. I'm using y-modem 'loady' to load the binary and 'go' to run it.
According to the discussion here, I used load address same as that of env variable 'load_addr' (0x82000000). I don't know what is going wrong here.
When I see the _start address of the binary using objdump, it is showing the same address. So, every time I'm able to load the binary but unable to run it.
Even I tried with standalone example from uboot sources too.
Here are the commands I used:
loady 0x82000000
go 0x82000000
Any help would be greatly appreciated.
Thanks,
Mani.