According to the software manifest for the Processor SDK 03.00.00.04 for 66AK2L06, avahi 0.6.32-r0.8 packages are included in this release. But in the target filesystem tar files that are included in this version of SDK, there are no avahi libraries or binaries present. I do see the precompiled avahi files under the linux-devkit/ directory of the SDK installed on the host.
How can I install the avahi package that's included in the linux-devkit onto the target filesystem so that we can run it on the target?