Tool/software: TI C/C++ Compiler
Hello, I'm trying to develop a GTK+ project in CCSv6 for an AM57x EVM (with the linux processor-sdk), and I'm running into some issues with the library dependencies of GTK+3.0. Essentially, I need to be able to add the libraries to the compiler (arm-linux-gnueabihf), so that it will actually compile if I put in #include<gtk/gtk.h> as I would in gcc.
In CCSv6 I've gone through the Properties -> C/C++ Build -> Cross G++ Linker -> Libraries and added all of the required libraries (from a pkg-config --libs gtk+3.0 call). I have also added the folder include paths necessary to build a GTK+ application. I then went to build the application, and the libraries were not included in the console output, which makes me think they were never part of the compilation process.
I have also tried to add the `pkg-config --libs gtk+-3.0` call to the compiler, which works on my terminal, but not on the compiler call. It apparently cannot find the gtk+-3.0 package, even if I include the folder that has the gtk+-3.0.pc file.
I'm sure this is a relatively simple issue, really all I want is to be able to use the GTK+ libraries included with the linux processor SDK with the G++ cross-compiler.