Hi,
I have installed linux dvsdk 4.00 for 3730.
Now when i run the script.sh file as given in the SDG --- using the command -- ${DVSDK}/setup.sh
At one point I get this error :
Since the script you are attempting to invoke has been converted to an
Upstart job, you may also use the restart(8) utility, e.g. restart acpid
acpid start/running, process 6776
/var/lib/dpkg/info/crossplatformui.postinst: line 106: cd: /usr/local/bin/ztemtApp/zteusbserial/2.6.32: No such file or directory
dpkg: error processing crossplatformui (--configure):
subprocess installed post-installation script returned error exit status 1
Errors were encountered while processing:
crossplatformui
E: Sub-process /usr/bin/dpkg returned an error code (1)
Failed setup, aborting..
Failed setup, aborting..
root@ubuntu:~/ti-dvsdk_dm3730-evm_4_00_00_22# ^C
I am new to linux and confused and stuck....
Kindly help please.....