hi :
I use dvrrdk decode_display_mcfw_demo to decode some h264 videos. it works,but display by hdmi image scintillation.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi :
I use dvrrdk decode_display_mcfw_demo to decode some h264 videos. it works,but display by hdmi image scintillation.
yes, thanks! In fact I don't know whether is interlaced H264 stream leads to the problem. but this stream really do exist the problem!
pls here: http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/177281.aspx#640742
I have tried the stream you shared on DVR RDK 3.5 release. It plays fine and I was not able to see any artifacts .The following changes were required to get the stream functional:
The stream you shared has issues
It does not start with SPS/PP. Cut the stream such that it starts with SPS/PPS.
Changes in ini file:
displaydelay= 4 (Stream has 4 reference frames)
numbuf = 10 (As 4 buffers are locked , need more output buffers)
width = 1920
height = 1080
Changes in multich_vdec_vdis.c
mulich_vdec_vdis_set_avsync_vidque_prm()
Change
queCfg->avsyncEnable = TRUE;
to
queCfg->avsyncEnable = FALSE;
This change is required due to a demo issue where timestamps are not set correctly for the elementary stream. This will not be an issue with real application which sets correct timestamp.
Changes in multich_vdec_vdis.c
MultiCh_createVdecVdis()
Change:
decPrm.chCreateParams[i].processCallLevel = VDEC_FRAMELEVELPROCESSCALL;
to
decPrm.chCreateParams[i].processCallLevel = VDEC_FIELDLEVELPROCESSCALL;
This is to enable decoding of interlaced content
Thank you very much,Badri Narayanan, you gave me a lot of help!
Pls post the query in DM816x or DM814x forum depending on the platform you are using along with failure logs and steps you are following.
DM814x forum: http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716.aspx
DM816x forum: http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717.aspx
The experts who can resolve the issue monitor the forum and would be able to provide the right answer